Part Number: DP83869HM
HI,
I have a question for you.When reading the DP83869HM chip register, it was found that 0X1DF (OP_MODE_DECODE) register was read back with the value of 0XFFFF. The following list is the value of the register read by me:
Register 0000 is: 1140
Register 0001 is: 7949
Register 0002 is: 2000
Register 0003 is: A0F1
Register 0004 is: 01E1
Register 0005 is: 0000
Register 01DF is: FFFF
I used the following sections from the datasheet and EVM user manual:
How do I configure to read the OP_MODE_DECODE(0X1DF) register correctly?
Regards,
Johnny