Part Number: TPS65988
Hi,
We are using TPS65988 in our project.
What will be the default Power negotiation between the TPS65988 and the external device before we have configured anything in the SPI Flash?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS65988
Hi,
We are using TPS65988 in our project.
What will be the default Power negotiation between the TPS65988 and the external device before we have configured anything in the SPI Flash?
Hi Baghiya,
The default configuration will depend on the ADCIN1 pin and the SPI_MISO pin, the specific configurations are outlined in section 8.4 of the TPS65988 datasheet.
Thank you,
Hari
Hi Hari,
That is the initial Boot configuration.
I am asking about the event before that. What will be the negotiation before anything is written on the SPI Flash?
Hi Baghiya,
I'm not sure I am understanding correctly, could you expand a bit on that, as in dead-battery condition or something else?
Upon boot up, the PD controller's ADC_IN1 and MISO pin will be checked to see which configuration to go into, sink/source, UFP/DFP, etc.Once that's configured, then it will establish a PD contract with the other device.There won't necessarily be a PD negotiation happening before that.
Thank you,
Hari
Hi Hari,
In case, the USB Port is in the SINK role.
So if there is no configuration file in the external SPI Flash. The TPS65988 will not allow any power to the system Or will it be in default state 5V@500/900mA.
Baghiya,
The USB Port can be put into Sink Role for 5V, 900mA capability if you have configured ADC_IN1 to be between 0.2-0.28 and SPI_MISO is 0 to select default configuration 2 which would happen right from the start if there was no program on SPI.
Thank you,
Hari