Part Number: TMDS181
Hi Sir,
I am adjusting the HDMI1.4 4k30p EYE pattern with TMDS181.
In the HW setting, EQ_SEL=Adaptive EQ, PRE_SEL=L,
When Vsadj=5.3kOhm, the level passed the compliance test.
However, I want to expand EYE a little more because the EYE pattern is at the limit.
In the HW setting, EQ_SEL=Adaptive EQ, PRE_SEL=L,
When Vsadj=3.6kOhm, EYE spread, but
CTS.7-2 VL level becomes low and it fails.
Isn't there a good way to keep VL level while spreading EYE?
Although detailed measurement data is condifential information, it is shared with TI Japan, so please contact TI Japan.