Part Number: SN65DSI86
Hello TI:
I want to use DSI86 to implement aux with IIC to read/write vcom of panel.
The TCOM vender release some document for me.
ex:
1.WriteDPCD(DPCD0048B,0x90);
2.WriteDPCD(DPCD0048E,0x9F);
3.IICWrite(0x9E,0x0F);
4.IICWrite(0x46,0x0A,0x5c);
Now , I think DSI86 reg setting is as follows:
1. aux_cmd=0x08, aux_addr[19:0]=0x0048B, aux_length[6:0]=0x01,Data0=0x90;
2.aux_cmd=0x08, aux_addr[19:0]=0x0048E, aux_length[6:0]=0x01,Data0=0x9F;
3.aux_cmd=0x04 or 0x00? , aux_addr[19:0]=? , aux_length[6:0]=? ,Data0=?
4.aux_cmd=0x04 or 0x00? , aux_addr[19:0]=? , aux_length[6:0]=? ,Data0=?
My question is I don't know how to set the reg to implement I2C-Over-Aux?
And if the setting of No1 & No2 is right?