Part Number: DP83TC811S-Q1
Other Parts Discussed in Thread: DP83TC811
Hi Team,
May I ask two questions of 811?
- Does the current DP83TC811 100M PHY support AVB protocol, or some protocols, such as IEEE802.AS (gPTP) protocol?
-
Is there any way to check whether the INT pin function is normal during production?
For example, after the SELF TEST function is turned on, INT generates an interrupt signal, allowing the master to detect this signal and determine that the INT pin function is OK.