Part Number: TUSB4020BI
Hi Team,
My customer is trying to carry out the downstream mask tests (of the USB 2.0 compliance tests) on the TUSB4020BI. However they are running into the issue that whenever they set the upstream device in the "Test packet mode" the test packets are not sent downstream by the USB hub.
With the oscilloscope they've verified the presence of the test packet on the internal bus from the upstream device into the TUSB4020BI, but no signal comes out on either of the outputs. This happens both when a downstream device (USB-stick) is connected and when no downstream device is connected.
Other data than the test packet does appear on the downstream path when a downstream device is connected.
Hence their questions:
Does the USB hub need to be put in a special mode to be able to forward the test packets from the upstream device?
And if so, how would this have to be done?
Thanks and looking forward to your response.
KR, Obinna.