This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB1064: Abnormal voltage level of SBU of TUSB1064

Part Number: TUSB1064
Other Parts Discussed in Thread: TUSB564, TPD8S300A

Hi team,

My customer is moving from TUSB564  TUSB1064 for gen2 solution.

And, they are using the same I2C configuration setting as the TUSB564 which has mass production already.

But the new gen2 project there is no AUX output because of that abnormal voltage level of SBU pin. It is only at 1.6v. 

As my understanding, the configuration setting of TUSB564 and TUSB1064 is almost the same. May I know there is any reason to induce the abnormal sbu voltage of TUSB1064? There is only TPD8s300A between type-c connector and TUSB1064. Thanks.