Part Number: TUSB1002A
Hello team,
My customer is designing with TUSB1002A and we have a few questions regarding AC caps:
- In datasheet section 6.5 there is a defined maximum AC coupling capacitance of 265nF. What are the consequences of exceeding this value? Customer host recommendation is the placement of 330nF capacitors along the TXP2/TXN2 pair and 220nF capacitors along the RXP1/RXN1 pair. I think the RX1 is fine, not sure about TX2 however.
- Also, hhould the capacitance on either side match? For example, should the AC coupling capacitance on RXP1 and TXP1 be the same? What would be the consequences of a mismatch in capacitance?