Part Number: DP83825I
Dear experts,
We have a custom iMX6ULL board on an m2 form factor. It is plugged to a MAIN board which contains the DP83825IRMQR eth phy chip, the magnetics, and the eth port. The ethernet chip uses an external 25MHz oscillator for clock.
The problem we are having is that the network connection of the ethernet chip flaps (turns on / off)
[ 959.561827] TI DP83825S 2188000.ethernet-1:00: attached PHY driver [TI DP83825S] (mii_bus:phy_addr=2188000.ethernet-1:00, irq=POLL)
[ 961.624018] fec 2188000.ethernet eth0: Link is Up - 100Mbps/Full - flow control rx/tx
[ 961.624212] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
[ 1062.503554] fec 2188000.ethernet eth0: Link is Down
[ 1063.543970] fec 2188000.ethernet eth0: Link is Up - 100Mbps/Full - flow control rx/tx
[ 1089.543566] fec 2188000.ethernet eth0: Link is Down
[ 1090.584208] fec 2188000.ethernet eth0: Link is Up - 100Mbps/Full - flow control rx/tx
[ 1115.543529] fec 2188000.ethernet eth0: Link is Down
[ 1116.583998] fec 2188000.ethernet eth0: Link is Up - 100Mbps/Full - flow control rx/tx
[ 1172.743596] fec 2188000.ethernet eth0: Link is Down
[ 1173.784015] fec 2188000.ethernet eth0: Link is Up - 100Mbps/Full - flow control rx/tx
[ 1263.223543] fec 2188000.ethernet eth0: Link is Down
[ 1264.263994] fec 2188000.ethernet eth0: Link is Up - 100Mbps/Full - flow control rx/tx
[ 1295.463566] fec 2188000.ethernet eth0: Link is Down
[ 1296.504006] fec 2188000.ethernet eth0: Link is Up - 100Mbps/Full - flow control rx/tx
root@localhost:~#
Our u-boot version is
VERSION = 2018
PATCHLEVEL = 03
SUBLEVEL =
EXTRAVERSION =
NAME =
and our Linux version is
root@localhost:~# cat /etc/*release; uname -a
DISTRIB_ID=Ubuntu
DISTRIB_RELEASE=16.04
DISTRIB_CODENAME=xenial
DISTRIB_DESCRIPTION="Ubuntu 16.04.6 LTS"
NAME="Ubuntu"
VERSION="16.04.6 LTS (Xenial Xerus)"
ID=ubuntu
ID_LIKE=debian
PRETTY_NAME="Ubuntu 16.04.6 LTS"
VERSION_ID="16.04"
HOME_URL="http://www.ubuntu.com/"
SUPPORT_URL="http://help.ubuntu.com/"
BUG_REPORT_URL="bugs.launchpad.net/.../"
VERSION_CODENAME=xenial
UBUNTU_CODENAME=xenial
Linux localhost 5.4.3-dirty #3 SMP Sun Aug 16 10:01:41 PST 2020 armv7l armv7l armv7l GNU/Linux
The connection of the DP83825 to the MAIN board is (sorry for the overlapping texts)
and to the m2 connector

While the connection on the iMX6ULL m2 edge finger is
to the iMX6ULL chip

Our device tree script in u-boot is imx6ull-prox-sodimm.dts (attached)
&fec1 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_enet1>;
phy-mode = "rmii";
phy-handle = <ðphy0>;
/*phy-reset-gpios = <&gpio1 5 0>;*/
status = "okay";
mdio {
#address-cells = <1>;
#size-cells = <0>;
ethphy0: ethernet-phy@0 {
compatible = "ethernet-phy-ieee802.3-c22";
reg = <0>;
clocks = <&clks IMX6UL_CLK_ENET_REF>;
/*clock-names = "rmii-ref";*/
clock-names = "no_enet_out";
assigned-clock-rates = <0>, <100000000>;
};
};
};
pinctrl_enet1: enet1grp {
fsl,pins = <
MX6UL_PAD_ENET1_RX_DATA0__ENET1_RDATA00 0x000110B0
MX6UL_PAD_ENET1_RX_DATA1__ENET1_RDATA01 0x000110B0
MX6UL_PAD_ENET1_RX_EN__ENET1_RX_EN 0x000110B0
MX6UL_PAD_ENET1_RX_ER__ENET1_RX_ER 0x000110B0
MX6UL_PAD_ENET1_RX_DATA0__PWM1_OUT 0x110b0
/*MX6UL_PAD_ENET1_TX_CLK__ENET1_TX_CLK 0x40000001*/
MX6UL_PAD_ENET1_TX_CLK__ENET1_REF_CLK1 0x40000001
MX6UL_PAD_ENET1_TX_DATA0__ENET1_TDATA00 0x000110B0
MX6UL_PAD_ENET1_TX_DATA1__ENET1_TDATA01 0x000110B0
MX6UL_PAD_ENET1_TX_EN__ENET1_TX_EN 0x000110B0
MX6UL_PAD_GPIO1_IO06__ENET1_MDIO 0x000110B0
MX6UL_PAD_GPIO1_IO07__ENET1_MDC 0x000110B0
>;
};
There is no driver yet for DP83825 in u-boot (as TI informed) so we are testing straight to Linux.
The DP83825 driver in Linux is dp83822.c (modified to include DP83825) (attached also).
Here are some of the logs in Linux
root@localhost:~# ethtool eth0
Settings for eth0:
Supported ports: [ TP MII ]
Supported link modes: 10baseT/Half 10baseT/Full
100baseT/Half 100baseT/Full
Supported pause frame use: Symmetric
Supports auto-negotiation: Yes
Advertised link modes: 10baseT/Half 10baseT/Full
100baseT/Half 100baseT/Full
Advertised pause frame use: Symmetric
Advertised auto-negotiation: Yes
Link partner advertised link modes: 10baseT/Half 10baseT/Full
100baseT/Half 100baseT/Full
Link partner advertised pause frame use: Symmetric Receive-only
Link partner advertised auto-negotiation: Yes
Speed: 100Mb/s
Duplex: Full
Port: MII
PHYAD: 0
Transceiver: external
Auto-negotiation: on
Supports Wake-on: g
Wake-on: d
Link detected: yes
root@localhost:~#
root@localhost:~# ethtool -S eth0
NIC statistics:
tx_dropped: 0
tx_packets: 17
tx_broadcast: 7
tx_multicast: 10
tx_crc_errors: 0
tx_undersize: 0
tx_oversize: 0
tx_fragment: 0
tx_jabber: 0
tx_collision: 0
tx_64byte: 0
tx_65to127byte: 10
tx_128to255byte: 0
tx_256to511byte: 7
tx_512to1023byte: 0
tx_1024to2047byte: 0
tx_GTE2048byte: 0
tx_octets: 3258
IEEE_tx_drop: 0
IEEE_tx_frame_ok: 17
IEEE_tx_1col: 0
IEEE_tx_mcol: 0
IEEE_tx_def: 0
IEEE_tx_lcol: 0
IEEE_tx_excol: 0
IEEE_tx_macerr: 0
IEEE_tx_cserr: 0
IEEE_tx_sqe: 0
IEEE_tx_fdxfc: 0
IEEE_tx_octets_ok: 3258
rx_packets: 0
rx_broadcast: 0
rx_multicast: 0
rx_crc_errors: 0
rx_undersize: 0
rx_oversize: 0
rx_fragment: 0
rx_jabber: 0
rx_64byte: 0
rx_65to127byte: 0
rx_128to255byte: 0
rx_256to511byte: 0
rx_512to1023byte: 0
rx_1024to2047byte: 0
rx_GTE2048byte: 0
rx_octets: 0
IEEE_rx_drop: 0
IEEE_rx_frame_ok: 0
IEEE_rx_crc: 0
IEEE_rx_align: 0
IEEE_rx_macerr: 0
IEEE_rx_fdxfc: 0
IEEE_rx_octets_ok: 0
root@localhost:~#
/* When connection is up */
root@localhost:~# ethtool -a eth0
Pause parameters for eth0:
Autonegotiate: on
RX: off
TX: off
RX negotiated: on
TX negotiated: on
root@localhost:~#
root@localhost:~# ethtool -i eth0
driver: fec
version: Revision: 1.0
firmware-version:
expansion-rom-version:
bus-info: eth0
supports-statistics: yes
supports-test: no
supports-eeprom-access: no
supports-register-dump: yes
supports-priv-flags: no
root@localhost:~#
root@localhost:~# ethtool -d eth0
Offset Values
------ ------
0x0000: 00 00 00 00 00 00 00 00 aa 00 80 0a 00 00 00 00
0x0010: 00 00 00 01 00 00 00 00 00 00 00 00 00 00 00 00
0x0020: 00 00 00 00 12 01 00 f0 00 00 00 00 00 00 00 00
0x0030: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0040: 6d 78 06 60 1a 00 00 00 00 00 00 00 00 00 00 00
0x0050: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0060: 00 00 00 00 00 00 00 40 00 00 00 00 00 00 00 00
0x0070: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0080: 00 00 00 00 24 01 c0 47 00 00 00 00 00 00 00 00
0x0090: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x00a0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x00b0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x00c0: 00 00 00 00 04 00 00 00 00 00 00 00 00 00 00 00
0x00d0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x00e0: 00 00 00 00 9d 44 ca 9a 08 88 4a b5 f0 ff 01 00
0x00f0: 0e 08 80 cc ff ff ff ff ff ff ff ff 00 00 00 00
0x0100: 0e 08 80 cc ff ff ff ff ff ff ff ff 00 00 00 00
0x0110: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0120: 00 00 40 00 08 00 80 00 00 00 00 00 00 00 00 00
0x0130: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0140: 00 00 00 00 00 01 00 00 00 00 00 00 00 00 00 00
0x0150: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0160: ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff
0x0170: ff ff ff ff ff ff ff ff 00 00 00 00 00 00 00 00
0x0180: 00 80 00 8e 00 c0 00 8e c0 07 00 00 00 00 00 00
0x0190: 10 00 00 00 84 00 00 00 08 00 00 00 08 00 00 00
0x01a0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x01b0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x01c0: 00 00 00 00 86 00 00 00 ff ff ff ff ff ff ff ff
0x01d0: 00 00 00 00 00 00 00 00 ff ff ff ff ff ff ff ff
0x01e0: ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff
0x01f0: ff ff ff ff 00 00 00 00 00 00 00 00 00 00 00 00
0x0200: 00 00 00 00 03 00 00 00 01 00 00 00 02 00 00 00
0x0210: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0220: 00 00 00 00 00 00 00 00 00 00 00 00 02 00 00 00
0x0230: 00 00 00 00 01 00 00 00 00 00 00 00 00 00 00 00
0x0240: 00 00 00 00 16 02 00 00 00 00 00 00 03 00 00 00
0x0250: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0260: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0270: 00 00 00 00 16 02 00 00 00 00 00 00 00 00 00 00
0x0280: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0290: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x02a0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x02b0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x02c0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x02d0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x02e0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x02f0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0300: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0310: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
.
. [up to]
.
0x3ff0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
root@localhost:~#
/* When connection is down */
root@localhost:~# ethtool -a eth0
Pause parameters for eth0:
Autonegotiate: on
RX: off
TX: off
root@localhost:~# dmesg | tail -50
[ 41.206908] kobject: 'vcsa5' ((ptrval)): kobject_uevent_env
[ 41.206983] kobject: 'vcsa5' ((ptrval)): fill_kobj_path: path = '/devices/virtual/vc/vcsa5'
[ 41.777350] kobject: 'vcs6' ((ptrval)): kobject_add_internal: parent: 'vc', set: 'devices'
[ 41.823704] kobject: 'vcs6' ((ptrval)): kobject_uevent_env
[ 41.823791] kobject: 'vcs6' ((ptrval)): fill_kobj_path: path = '/devices/virtual/vc/vcs6'
[ 41.826730] kobject: 'vcsu6' ((ptrval)): kobject_add_internal: parent: 'vc', set: 'devices'
[ 41.843530] kobject: 'vcsu6' ((ptrval)): kobject_uevent_env
[ 41.843618] kobject: 'vcsu6' ((ptrval)): fill_kobj_path: path = '/devices/virtual/vc/vcsu6'
[ 41.844077] kobject: 'vcsa6' ((ptrval)): kobject_add_internal: parent: 'vc', set: 'devices'
[ 41.850598] kobject: 'vcsa6' ((ptrval)): kobject_uevent_env
[ 41.850682] kobject: 'vcsa6' ((ptrval)): fill_kobj_path: path = '/devices/virtual/vc/vcsa6'
[ 42.189044] kobject: 'imx!sdma!sdma-imx6q.bin' ((ptrval)): kobject_uevent_env
[ 42.189149] kobject: 'imx!sdma!sdma-imx6q.bin' ((ptrval)): fill_kobj_path: path = '/devices/soc0/soc/2000000.aips-bus/20ec000.sdma/firmware/imx!sdma!sdma-imx6q.b'
[ 42.194998] kobject: 'firmware' ((ptrval)): kobject_cleanup, parent (ptrval)
[ 42.195063] kobject: 'firmware' ((ptrval)): calling ktype release
[ 42.195139] kobject: 'firmware': free name
[ 42.195191] kobject: 'imx!sdma!sdma-imx6q.bin' ((ptrval)): kobject_cleanup, parent (ptrval)
[ 42.195239] kobject: 'imx!sdma!sdma-imx6q.bin' ((ptrval)): calling ktype release
[ 42.195313] kobject: 'imx!sdma!sdma-imx6q.bin': free name
[ 42.195428] imx-sdma 20ec000.sdma: external firmware not found, using ROM firmware
[ 44.509952] FAT-fs (mmcblk0p2): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
[ 49.314371] TI DP83825S 2188000.ethernet-1:00: attached PHY driver [TI DP83825S] (mii_bus:phy_addr=2188000.ethernet-1:00, irq=POLL)
[ 49.338710] kobject: 'wakeup0' ((ptrval)): kobject_uevent_env
[ 49.338816] kobject: 'wakeup0' ((ptrval)): fill_kobj_path: path = '/devices/soc0/soc/2100000.aips-bus/2188000.ethernet/net/eth0/wakeup0'
[ 49.383916] kobject: 'wakeup0' ((ptrval)): kobject_cleanup, parent (ptrval)
[ 49.383974] kobject: 'wakeup0' ((ptrval)): calling ktype release
[ 49.384151] kobject: 'wakeup0': free name
[ 51.909389] new mount options do not match the existing superblock, will be ignored
[ 52.139015] kobject: '0:26' ((ptrval)): kobject_add_internal: parent: 'bdi', set: 'devices'
[ 52.140012] kobject: '0:26' ((ptrval)): kobject_uevent_env
[ 52.140100] kobject: '0:26' ((ptrval)): fill_kobj_path: path = '/devices/virtual/bdi/0:26'
[ 54.189303] new mount options do not match the existing superblock, will be ignored
[ 65.624226] random: crng init done
[ 915.625989] fec 2188000.ethernet eth0: Link is Up - 100Mbps/Full - flow control rx/tx
[ 915.627066] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
[ 959.561827] TI DP83825S 2188000.ethernet-1:00: attached PHY driver [TI DP83825S] (mii_bus:phy_addr=2188000.ethernet-1:00, irq=POLL)
[ 961.624018] fec 2188000.ethernet eth0: Link is Up - 100Mbps/Full - flow control rx/tx
[ 961.624212] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
[ 1062.503554] fec 2188000.ethernet eth0: Link is Down
[ 1063.543970] fec 2188000.ethernet eth0: Link is Up - 100Mbps/Full - flow control rx/tx
[ 1089.543566] fec 2188000.ethernet eth0: Link is Down
[ 1090.584208] fec 2188000.ethernet eth0: Link is Up - 100Mbps/Full - flow control rx/tx
[ 1115.543529] fec 2188000.ethernet eth0: Link is Down
[ 1116.583998] fec 2188000.ethernet eth0: Link is Up - 100Mbps/Full - flow control rx/tx
[ 1172.743596] fec 2188000.ethernet eth0: Link is Down
[ 1173.784015] fec 2188000.ethernet eth0: Link is Up - 100Mbps/Full - flow control rx/tx
[ 1263.223543] fec 2188000.ethernet eth0: Link is Down
[ 1264.263994] fec 2188000.ethernet eth0: Link is Up - 100Mbps/Full - flow control rx/tx
[ 1295.463566] fec 2188000.ethernet eth0: Link is Down
[ 1296.504006] fec 2188000.ethernet eth0: Link is Up - 100Mbps/Full - flow control rx/tx
root@localhost:~#
root@localhost:~# cat /etc/*release; uname -a
DISTRIB_ID=Ubuntu
DISTRIB_RELEASE=16.04
DISTRIB_CODENAME=xenial
DISTRIB_DESCRIPTION="Ubuntu 16.04.6 LTS"
NAME="Ubuntu"
VERSION="16.04.6 LTS (Xenial Xerus)"
ID=ubuntu
ID_LIKE=debian
PRETTY_NAME="Ubuntu 16.04.6 LTS"
VERSION_ID="16.04"
HOME_URL="http://www.ubuntu.com/"
SUPPORT_URL="http://help.ubuntu.com/"
BUG_REPORT_URL="bugs.launchpad.net/.../"
VERSION_CODENAME=xenial
UBUNTU_CODENAME=xenial
Linux localhost 5.4.3-dirty #3 SMP Sun Aug 16 10:01:41 PST 2020 armv7l armv7l armv7l GNU/Linux
root@localhost:~#
Thank you very much, experts.
Best regards,
Carlos