This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83TC811S-Q1: dp83tc811s-q1 Can the MDIO pin accept 1.8Kohm pull up resistor?

Part Number: DP83TC811S-Q1


Hi  Colleagues,

  customer are using the MAC module, so the pull up resistor on our MDIO pin is about 1.8K and can not be changed. My question is that if we can support this, our recommendation on the datasheet is 2.2k ohm to 9Kohm.

 also, i have reviewed the schematic ,and leaves my comments, could you please also help to review it since it is first time of my customer to use our automotive phy.

Best Regards

David Liu4477.eth.pdf