Part Number: TPS65981
Other Parts Discussed in Thread: TUSB1042I, HD3SS3220, TPS65982, TUSB542
We have a custom PCB that uses the TPS65981 as the PD controller to interface with an iPad. The configuration we require is for us to be the power source and the iPad to be the data source.
For Power I setup the TPS6591 to be a Initiate Swap Source and Process Swap Source so that our board supplies the power.
For Data Then I do Initiate Swap to UFP and Process Swap to UFP to make the iPad the data source.
This seems to work and I am fairly happy with the results. Our current system is USB2.0 which works fine for the TPS65981 data mux.
We are upgrading our system to USB3.0 superspeed. My question is what would TI recommend to upgrade my design from USB2.0 to USB3.0 dataspeeds and still keep the current PD functionality? Should I keep the TPS65981 for the PD controller and use another TI part such as the TUSB1042I to mux the USB3.0 data line? Or do I use a separate IC all together such as the HD3SS3220? Although it isn't clear if the HD3SS3220 can support the PD power and data swapping I require to support the power and data configuration that I require. Some guidance and suggestions would be appreciated.
Thank you.