Part Number: TPS65987D
Other Parts Discussed in Thread: TPS65987
Hi Team,
We are working with TPS65987 and have a question regarding the allowable load capacitance. In the datasheet, table 27 on page 54 specifies an absolute max of 120uF capacitance on a PowerPath used as a sink. Is this a limitation of the TPS65987 itself, or a limitation imposed by USB-C specifications? I noticed that even the dev board has at least ~350uF of capacitance on whichever of the power paths is connected to SYS_PWR (dev board schematic page 12, "Fast Role Swap caps" plus others) -- and the dev board works fine. In the design we have greater than 120uF and do not want to run into issues.
Thank you!
Garret