Part Number: TPS65988DJ
Other Parts Discussed in Thread: BQ25703A, TPS65988
Hi,
I'm using the TPS65988DJ to design a dual port, USB-C battery bank, with one port being bi-direction to charge the battery bank itself. PP_HV1 is connected to a charger based on the BQ25703A chip while PP_HV2 will be supplied by buck/boost device with I2C interface. I have some simple question;
1. Some application notes shows external MOSFET switches for power paths while the datasheet of the TPS65988DJ states that the internal switches are bi-directional. Can the internal switches of the TPS65988DJ be used for both source and sink depending if I want to charge the power bank or supply a device?
2. Is an external EEPROM needed to hold the configuration settings as illustrated in application note SLVAE18 or will they be stored in the TPS65988DJ chip?
3. How should I damp the configurations? Can I connect an EV2300 to I2C2 of the TPS65988DJ to program the configurations?
Thanks