Part Number: TVP5146M2
Other Parts Discussed in Thread: TVP5146
Hi All
I am trying to capture a movie from TVP5146 analog video decoder from TVP5146 module on AM5728-evm, and I use 'ti-processor-sdk-linux-am57xx-evm-06.03.00.106' SDK. I followed 'AM5728 VIP and V4L2 interface with TVP5146 Analog Video Decoder Problem' thread, and now I can see these messages on 'dmesg' output.
[ 3.547762] tvp514x 4-005d: tvp514x 4-005d decoder driver registered !! ... [ 71.493672] vin3a: Port A: Using subdev tvp514x 4-005d for capture [ 71.556900] vin3a: matched fourcc: UYVY: code: 2006 idx: 0 [ 71.556908] vin3a: matched fourcc: YUYV: code: 2006 idx: 1 [ 71.556915] vin3a: matched fourcc: VYUY: code: 2006 idx: 2 [ 71.556922] vin3a: matched fourcc: YVYU: code: 2006 idx: 3 ... [ 71.569860] vin3a-0: device registered as video1 [ 71.591215] vin3a-0: device registered as video2 [ 71.605026] vin3a-0: device registered as video3 [ 71.621337] vin3a-0: device registered as video4 ... [ 80.214845] vin3a: subdev default mbus_fmt 0000 is not matched. [ 80.267339] vin3a: init_port set_fmt failed in subdev: (-22) [ 80.267346] vin3a: vip_init_port: g_mbus_fmt subdev mbus_code: 2006 fourcc:UYVY size: 0x0 [ 80.267396] vin3a: calc_format_size: fourcc:UYVY size: 128x128 bpl:256 img_size:32768 [ 80.267404] vin3a-0: init_stream fourcc:UYVY size: 128x128 bpl:256 img_size:32768 [ 80.267408] vin3a-0: init_stream vpdma data type: 0x27 [ 80.267414] vin3a-0: vip_init_stream: stream instance 0x00000000ec495000 [ 80.303069] vin3a: calc_format_size: fourcc:UYVY size: 128x128 bpl:256 img_size:32768 [ 80.303078] vin3a-0: init_stream fourcc:UYVY size: 128x128 bpl:256 img_size:32768 [ 80.303082] vin3a-0: init_stream vpdma data type: 0x27 [ 80.303088] vin3a-0: vip_init_stream: stream instance 0x00000000ec497000 [ 80.329235] vin3a-0: init_stream fourcc:UYVY size: 128x128 bpl:256 img_size:32768 [ 80.329239] vin3a-0: init_stream vpdma data type: 0x27 [ 80.329246] vin3a-0: vip_init_stream: stream instance 0x00000000ec494000 [ 80.329314] vin3a: calc_format_size: fourcc:UYVY size: 128x128 bpl:256 img_size:32768 [ 80.329323] vin3a-0: init_stream fourcc:UYVY size: 128x128 bpl:256 img_size:32768 [ 80.329326] vin3a-0: init_stream vpdma data type: 0x27 [ 80.329333] vin3a-0: vip_init_stream: stream instance 0x00000000ec496000 [ 80.386710] vin3a-0: vip_release [ 80.411004] vin3a-0: vip_release_stream: stream instance 0x186bfccdec495000 [ 80.412996] vin3a-0: vip_release [ 80.413015] vin3a-0: vip_release_stream: stream instance 0x186bfccdec497000 [ 80.432817] vin3a-0: vip_release_stream: stream instance 0x186bfccdec496000 [ 80.488057] vin3a-0: vip_release [ 80.488079] vin3a-0: vip_release_stream: stream instance 0x186bfccdec494000 [ 80.488085] vin3a: vip_release_port: port instance 0x186bfccded781040
When I run a Yavta command 'yavta -c60 -fUYVY -Fvout_720x576_yuyv.yuv -s720x576 /dev/video1', the system fails to set format:
Device /dev/video1 opened. Device `vip' on `platform:vip2:vin3a:stream0' is a video output (without mplanes) device. Unable to set format: Invalid argument (22).
The 'dmesg' output after the execution of yavta command is as below:
[ 1460.287542] vin3a-0: vip_open [ 1460.312409] vin3a: subdev default mbus_fmt 0000 is not matched. [ 1460.341420] vin3a: init_port set_fmt failed in subdev: (-22) [ 1460.341425] vin3a: vip_init_port: g_mbus_fmt subdev mbus_code: 2006 fourcc:UYVY size: 0x0 [ 1460.341471] vin3a: calc_format_size: fourcc:UYVY size: 128x128 bpl:256 img_size:32768 [ 1460.341479] vin3a-0: init_stream fourcc:UYVY size: 128x128 bpl:256 img_size:32768 [ 1460.341482] vin3a-0: init_stream vpdma data type: 0x27 [ 1460.341488] vin3a-0: vip_init_stream: stream instance 0x00000000ec494000 [ 1460.424091] vin3a-0: s_fmt input fourcc:UYVY size: 720x576 bpl:0 img_size:0 [ 1460.424099] vin3a-0: try_fmt fourcc:UYVY size: 720x576 [ 1460.424120] vin3a-0: try_fmt best subdev size: 0x0 [ 1460.424138] vin3a: calc_format_size: fourcc:UYVY size: 128x128 bpl:256 img_size:32768 [ 1460.424142] vin3a-0: s_fmt try_fmt fourcc:UYVY size: 128x128 bpl:256 img_size:32768 [ 1460.424168] vin3a-0: s_fmt fourcc:UYVY size: 128x128 bpl:256 img_size:32768 [ 1460.424173] vin3a-0: s_fmt pix_to_mbus mbus_code: 2006 size: 0x0 [ 1460.453179] vin3a-0: set_fmt failed in subdev [ 1460.453246] vin3a-0: vip_release [ 1460.453264] vin3a-0: vip_release_stream: stream instance 0x186bfccdec494000 [ 1460.453271] vin3a: vip_release_port: port instance 0x186bfccded781040
I debuged the code, and I found that when the 'tvp514x_get_pad_format' is called, the 'filed', 'code', 'colorspace', 'width', and 'height' of the returned format is zero. Also 'tvp514x_set_pad_format' always returns 'EINVAL'. Can anyone help me to debug these two functions and find out why the system can't set the format?
I added some debug messages in the 'tvp514x_get_pad_format' and 'tvp514x_set_pad_format' of tvp514x.c file as follow:
static int tvp514x_set_pad_format(struct v4l2_subdev *sd,
struct v4l2_subdev_pad_config *cfg,
struct v4l2_subdev_format *fmt)
{
struct tvp514x_decoder *decoder = to_decoder(sd);
v4l2_info(sd, "Ali-Debug start %s !!\n", __func__);
v4l2_info(sd, "Ali-Debug %d, %d !!\n", fmt->format.field, V4L2_FIELD_INTERLACED);
v4l2_info(sd, "Ali-Debug %d, %d !!\n", fmt->format.code, MEDIA_BUS_FMT_UYVY8_2X8);
v4l2_info(sd, "Ali-Debug %d, %d !!\n", fmt->format.colorspace, V4L2_COLORSPACE_SMPTE170M);
v4l2_info(sd, "Ali-Debug %ld, %ld !!\n", fmt->format.width, tvp514x_std_list[decoder->current_std].width);
v4l2_info(sd, "Ali-Debug %ld, %ld !!\n", fmt->format.height, tvp514x_std_list[decoder->current_std].height);
if (fmt->format.field != V4L2_FIELD_INTERLACED ||
fmt->format.code != MEDIA_BUS_FMT_UYVY8_2X8 ||
fmt->format.colorspace != V4L2_COLORSPACE_SMPTE170M ||
fmt->format.width != tvp514x_std_list[decoder->current_std].width ||
fmt->format.height != tvp514x_std_list[decoder->current_std].height)
return -EINVAL;
v4l2_info(sd, "Ali-Debug end %s !!\n", __func__);
decoder->format = fmt->format;
return 0;
}
static int tvp514x_get_pad_format(struct v4l2_subdev *sd,
struct v4l2_subdev_pad_config *cfg,
struct v4l2_subdev_format *format)
{
v4l2_info(sd, "Ali-Debug start %s !!\n", __func__);
struct tvp514x_decoder *decoder = to_decoder(sd);
__u32 which = format->which;
if (format->pad)
return -EINVAL;
v4l2_info(sd, "Ali-Debug %d !!\n", (which == V4L2_SUBDEV_FORMAT_ACTIVE));
v4l2_info(sd, "Ali-Debug %d, %d !!\n", decoder->format.field, V4L2_FIELD_INTERLACED);
v4l2_info(sd, "Ali-Debug %d, %d !!\n", decoder->format.code, MEDIA_BUS_FMT_UYVY8_2X8);
v4l2_info(sd, "Ali-Debug %d, %d !!\n", decoder->format.colorspace, V4L2_COLORSPACE_SMPTE170M);
v4l2_info(sd, "Ali-Debug %ld, %ld !!\n", decoder->format.width, tvp514x_std_list[decoder->current_std].width);
v4l2_info(sd, "Ali-Debug %ld, %ld !!\n", decoder->format.height, tvp514x_std_list[decoder->current_std].height);
if (which == V4L2_SUBDEV_FORMAT_ACTIVE) {
format->format = decoder->format;
return 0;
}
format->format.code = MEDIA_BUS_FMT_UYVY8_2X8;
format->format.width = tvp514x_std_list[decoder->current_std].width;
format->format.height = tvp514x_std_list[decoder->current_std].height;
format->format.colorspace = V4L2_COLORSPACE_SMPTE170M;
format->format.field = V4L2_FIELD_INTERLACED;
return 0;
}
And here is the output of dmesg
root@am57xx-evm:~# dmesg | grep 'Ali-Debug' [ 80.208283] tvp514x 4-005d: Ali-Debug start tvp514x_get_pad_format !! [ 80.220990] tvp514x 4-005d: Ali-Debug 1 !! [ 80.251948] tvp514x 4-005d: Ali-Debug 0, 4 !! [ 80.264053] tvp514x 4-005d: Ali-Debug 0, 8198 !! [ 80.272094] tvp514x 4-005d: Ali-Debug 0, 1 !! [ 80.300798] tvp514x 4-005d: Ali-Debug 0, 0 !! [ 80.336792] tvp514x 4-005d: Ali-Debug 0, 0 !! [ 80.405515] tvp514x 4-005d: Ali-Debug start tvp514x_set_pad_format !! [ 80.447949] tvp514x 4-005d: Ali-Debug 0, 4 !! [ 80.455601] tvp514x 4-005d: Ali-Debug 8198, 8198 !! [ 80.504178] tvp514x 4-005d: Ali-Debug 0, 1 !! [ 80.520343] tvp514x 4-005d: Ali-Debug 0, 0 !! [ 80.551447] tvp514x 4-005d: Ali-Debug 0, 0 !! [ 129.879144] tvp514x 4-005d: Ali-Debug start tvp514x_get_pad_format !! [ 129.887134] tvp514x 4-005d: Ali-Debug 1 !! [ 129.891249] tvp514x 4-005d: Ali-Debug 0, 4 !! [ 129.896001] tvp514x 4-005d: Ali-Debug 0, 8198 !! [ 129.900639] tvp514x 4-005d: Ali-Debug 0, 1 !! [ 129.905451] tvp514x 4-005d: Ali-Debug 0, 0 !! [ 129.909863] tvp514x 4-005d: Ali-Debug 0, 0 !! [ 129.914737] tvp514x 4-005d: Ali-Debug start tvp514x_set_pad_format !! [ 129.921226] tvp514x 4-005d: Ali-Debug 0, 4 !! [ 129.928232] tvp514x 4-005d: Ali-Debug 8198, 8198 !! [ 129.934122] tvp514x 4-005d: Ali-Debug 0, 1 !! [ 129.938617] tvp514x 4-005d: Ali-Debug 0, 0 !! [ 129.943025] tvp514x 4-005d: Ali-Debug 0, 0 !! [ 130.031589] tvp514x 4-005d: Ali-Debug start tvp514x_set_pad_format !! [ 130.038071] tvp514x 4-005d: Ali-Debug 1, 4 !! [ 130.042474] tvp514x 4-005d: Ali-Debug 8198, 8198 !! [ 130.047369] tvp514x 4-005d: Ali-Debug 1, 1 !! [ 130.051770] tvp514x 4-005d: Ali-Debug 0, 0 !! [ 130.056142] tvp514x 4-005d: Ali-Debug 0, 0 !!