Part Number: TCAN4550EVM
Other Parts Discussed in Thread: LAUNCHXL-CC3235S, TCAN4550, TCAN4550-Q1
Hello,
Customer is connecting the TCAN4550EVM with the LAUNCHXL-CC3235S,
As I understand 2 is a questions for the WIFI team, I will open a new post.
he has the following questions:
1.The SPI protocol reference code of the CC3235 ask for ready signal, I not sure if it is exist on the TCAN4550.
2. The SPI reference code are not transmit the data to the other side with WiFi, how should I do it?
3. I connected CANbus generator and sniffer to the TCAN4550, but there is no transaction, not on the SPI and not on the CANbus port.
Thanks.