Part Number: TCAN4550
HI,
I discovered the datasheet and there some missing information.
The Vsupply voltage range is 6-24V
The Isupply current for dominant in load bus is 90mA
The current reference for 90mA is according to 24V Vsup? if so, the power consumption of (0.09mA*24V = 2.16W) seems very high for this small device. Did I miss something?
I also calculate the Tj and for this value it seems unreasonable.
Tj = TA+(Rj*Power) = 125 + (35.2*90mA*24V) = 195.2
Also there any recomanded MCU to connecting with this controller?
Thanks in advance.
Tomer.