Part Number: SN65HVD24
Other Parts Discussed in Thread: STRIKE
Hi team,
this is brandon. in our before design, SN65HVD24 is linked directly on BUS, which cause the demage when Lighting happened. therefore, we intended to design the Lightning protection to protect our device.
the baisc design solution is shown as below picture:
we may want to know that whether it is ok to set the R at 10ohm with 0402 package? we also need to make sure that the signal quality should not be influence much with this design.the length of BUS is 250 meter and 84 node. Communication rate is 1Mbps and the Cable characteristic impedance is around 70-120ohm(Ordinary four-core wire).
could you also recommended the value of the resistance connected with 485 and the package size?
BR
Brandon