Other Parts Discussed in Thread: ISO1211
Hi,
I have a requirement to use a single set of Terminal Blocks to process both the AC and DC signals.
Opto-coupler Turn ON Voltage = 15 VDC, equivalent AC
The input can be either AC or DC, we do not want to turn-on the opto-coupler below 15 VDC = equivalent AC
When AC is used the the AC voltage will not be more than 250 VAC but if it, is it does not matter. We do not need to limit the top voltage.
I was wondering if there is a simple generic circuit that I can use for this space constraints application, thanks in advance.