Part Number: TPS25750EVM
I plan to use the module as a PD for an upstream device. I need to test USB-2 communication a FTDI serial chip. The evaluation module indicate the USB 2 lines are available on the expansion connector but the expansion connector (J11) is not described on the schematic so it is not clear on which pins to use.
The charging parts works fine.