Part Number: TPS65987D
Other Parts Discussed in Thread: TPS65987, , BQ24192I, TPS65988
1. Should C_USB_N and C_USB_P (pins 50,53) be tied to GND of left floating if BC1.2 support is not needed?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS65987D
Other Parts Discussed in Thread: TPS65987, , BQ24192I, TPS65988
1. Should C_USB_N and C_USB_P (pins 50,53) be tied to GND of left floating if BC1.2 support is not needed?
Hello,
I've assigned this issue to the relevant expert who will get back to you shortly
Dear Nir,
According to the datasheet, it is recommended to have 4.7uF on LDO_1V8.
I would recommend having the battery charger part reviewed on the Battery Charging Forum.
Thanks,
Mike Emanuel
Please click "This resolved my issue" button if this post answers your question.
Thank you Mike.
Just one thing is not yet clear to me: Say I wish to reach a 5A current sink on the TPS65987 (and I have the needed USB PD power supply for that)
I understand I will need to use the application customization tool to generate a binary file but what do I need
to have in terms of hardware and how do I download this file into the hardware is not clear to me yet.
Thank you,
Nir.
Adding to my last question:
Assuming I connect my host micro-controller via the I2C to the TPS65987, will I be able to control all of the device features by following
the "TPS65987DDH and TPS65988DH Host Interface Technical Reference Manual" (SLVUBH2B) document?
Nir.
Dear Nir,
You have two options.
The first is to use a Flash memory and program it following the GUI video below.
https://training.ti.com/tps6598x-application-customization-gui-tool-basic-introduction
The second is to use I2C. The following application note describes how to program using I2C and the flash.
"TPS65987 and TPS65988 SPI Flash Firmware Update Over I2C"
In addition, using the mentioned, "TPS65987DDH and TPS65988DH Host Interface Technical Reference Manual" will help as well.
Thanks,
Mike Emanuel
Please click "This resolved my issue" button if this post answers your question.
Dear Mike,
Thank you. Please find attached my updated schematics.
I have added connector J8 which will connect to the Aardvark I2C/SPI programmer's cable. I have also added U63 which is a flash device (same one as used in the Eval board of the TPS65987). I have
connected the SPI lines from the J8 connector to the SPI lines of the TPS65987 and to the Flash device.
My plan is to use the Application Customization Tool with the Aardvark programmer to program the Flash device with the needed TPS65987 configuration image.
Will this setup work?
Thank you,
Nir.
Dear Nir,
This should work. Please follow the schematic on page 10 of the "TPS65987 Evaluation Module" User Guide to connect the flash. I noticed some pullup resistors missing on CS and MISO.
Thanks,
Mike Emanuel
Please click "This resolved my issue" button if this post answers your question.