Other Parts Discussed in Thread: SN75LVDS83
The SN75LVDS83 and 86 pair is an 18 bit LVDS chip solution.
I am using A 4.3” TDT display which is 24 bits.
Now, I could ground two pins and go 18 bit on the
display and only use 6 bits from the MCU but I don’t know the implications of
that?
So, does TI offer a 24bit to 24 bit solution?
Q2) why are there 3YM and 3YP pins if they
aren’t transferred across the cable?
Are they used in another application that
is unique and not common, thus not shown. Also, is this the best pair of parts that
I should be looking at if it’s TI? What is the longevity? Is it for new
designs? Etc…. Thank you!