This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB9261-Q1: About the time until USB_DP becomes High after VBUS, 3.3V and 1.1V are turned on

Part Number: TUSB9261-Q1

Hi,

Please tell the specification of TUSB9261-Q1 about the time

until USB_DP  becomes High after VBUS, 3.3V and 1.1V are turned on at the same time.

Also, is the maximum value of the actual value less than 1 second (USB standard)?