Part Number: DS90UB954-Q1
Hello,
Is it possible to connect two ov2311 camera sensors(2MP 60fps) and stream in parallel ?
Currently i have connected one camera(ov2311 2MP) on deserializer and i am able to stream. I am planning to connect one more ov2311 camera(2MP 60fps) on second port of
deserializer, and stream in parallel.
Will there be any lag in steaming, because i am streaming from both the cameras in parallel.
OV2311 supports a one/two-lane MIPI transmitter interface with a data transfer rate of up to 800 Mbps per lane
Regards,
SHAMMI