Part Number: DS280MB810
Hello team,
Can DS280MB810 somehow operate up to 32Gbps(NRZ)?
With the device, signal will not pass at the rate? or signal will pass but it will not give enough performance as repeater?
Best regards,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS280MB810
Hello team,
Can DS280MB810 somehow operate up to 32Gbps(NRZ)?
With the device, signal will not pass at the rate? or signal will pass but it will not give enough performance as repeater?
Best regards,
Hi,
The DS280MB810 is a linear device and will continue to operate above 28 Gbps. At 32 Gbps the peak gain and bandwidth will no longer be optimal and the redriver performance will be reduced. The performance at 32 Gbps will be very sensitive to the application, so I cannot say what level of performance will still be available for a specific application.
Regards,
Lee