Dear Sir or Madam
I have four questions regarding the data sheet.
When inputting 24MHz with an oscillator, is it OK to think that the conditions for PPM (±100) and load capacitance (12-24pF) are the same as for the oscillator?
(Example: Input after VDD input, but before GRSTz rise.)
In addition, it seems that the data sheet for the USB hub only described the PowerON sequence as shown in the figure on the right. Please let me know if there is a regulation of Power OFF.
I was unable to read the slew rate or voltage level for the oscillator from the HSU hub data sheet.
Please let us know if this oscillator meets the HUB hub standards (whether the slew rate or voltage level is acceptable).
Please let me know if you have any regulations regarding communication start timing.
Yours sincerely,