Part Number: SN65LVP20
I have 2 questions about output drive/impedance for the SN65LVP20 LVPECL output.
1/ The differential transmission line is specified at 100 Ohms (90 to 132 Ohms), confirmed by 50 Ohms from both Y and Z to Vcc-2. Can the output drive a 50 Ohm impedance RF Transformer as ECL would normally drive a 50 Ohms differential load.
2/ Do both the differential outputs (Y and Z) require a pull-down resistor to GND as ECL emitter-followers normally require this. What would be the pull-down resistor values.
Regards,
Chris Heath