Part Number: TLK10002
Other Parts Discussed in Thread: TLK10034, TLK10031, TLK10232
We want to provide a 9.8 Gbps CPRI link towards the RRH. However, we know that the AIF2 interface on the TMS320TCI6638 can support only upto 4.9 Gbps. We want to combine the two AIF2 interfaces available from each DSP SoC and provide a 9.8 Gbps CPRI link. We are looking at TLK10002 for this purpose. We have three DSP SoCs for which this CPRI rate combining is to be done on the same RAC card.
Clarity required:
1. Since TLK10002 has two channels, do we need two devices to cater to the three DSP SoCs on the RAC card?
2. Is there any other equivalent device that you recommend, - is there a variant of this device which supports three channels so that we need to use only one device per RAC card?