Part Number: TCAN4550
Hi,
We are using TCAN4550 CAN interface in our IMX6ULL platform.
Initially when we tried to recieve the data in 1sec frequency, we got the "tcan4x5x spi0.0 can2: msg lost in rxf0" error.
Then we changed the "bosch,mram-cfg = <0x0 3 2 1 6 3 10 7>;" to "bosch,mram-cfg = <0x0 64 64 64 64 64 32 32>;" in dts file, then we are able to receive the CAN data upto every 15ms.
Our requirement is to recevice the CAN data in every 1ms.
When we tried to receive the CAN data from CAR in 1ms, we are getting "tcan4x5x spi0.0 can2: msg lost in rxf0" .
Please suggest to resolve this issue.
Regards,
Haji