This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRA829_SDK_LIN(based on uart)_Break_Field



Hi,

I Found diagnostic test for Lin in SDK(psdk_rtos_auto_j7_06_02_00_21),and read the code,but i don not understand how it handle the Break Field.It seems that two bytes(one is 0x00,the other is 0x20)  is transmitted.But there will be a stop bit(high) after 0x00 is transmitted,it can not be a solid break field(13 bit low).Can you please enlight me about this?

Regards,