Other Parts Discussed in Thread: TCAN1043, STRIKE, TCAN1043-Q1
Hi TI member,
Regarding the CAN wake-up function,
When do ESD discharge(± 4/6/8/15kV, ISO-10605) on CAN bus whatever contact and air. We found the ESD will cause the TCAN1043 trigger the INH lead to DUT wake-up.
Because the ESD clamping waveform will similar wake-up pattern(high -> low -> high) of TCAN1043. Interestingly, it will trigger when the negative current is on CAN_L, or the positive current is on CAN_H
Is the wake-up pattern can be adjusted? (ex. Increase the recognition of CAN device ID)
And do you have any suggest about this situation?
Thank you.
PS. CAN bus ESD protection diode is PESD1CAN-U.
Best Regards
Bruce Hsin