Part Number: PCA9306
Hello,
My customer is using PCA9306 as follows.
In normal operation, I2C master device (1.8V) communicate with I2C slave device (3.3V) via PCA9306.
During debug, the I2C master device is power down (1.8V power supply is off), and other I2C master devices for debugging purpose (3.3V) communicate with the I2C slave device directly.
Q1:
During debugging, 1.8V is off and 3.3V is on at PCA9306. Could this damage TPA9306? Or is this OK with no issue?
Q2:
During debugging, PCA9306 is still connected with 3.3V is on. The I2C master devices can communicate with the I2C slave devices with no issue?
Best regards,
K.Hirano