Part Number: DP83867CR
Ethernet defines a minimum idle period (IPG) between transmission of Ethernet packets. Gigabit Ethernet appears to allow a minimum received IPG of 8 bytes; however, in digital loopback the TI DP83867 appears to have a lower limit of 11 IPG bytes. We would like to confirm the DP83867 minimum IPG? We would also like to understand the two byte “preamble” that is required on the RGMII interface. Is the two byte preamble a part of the IPG bytes or is it in addition to the IPG?