Part Number: TCA9534
I am having difficulty communicating with the TCA9534. I am probing the I2C Clock and Data lines. I can see the Master has initiated the Start Condition. I can see that the slave address is clocked out. I can see the Write command bit is 0. The TCA9534 is not holding the Data Line low on the next clock cycle to provide an ACK. I have another I2C device working on this bus, so the bus is working. I am seeking help with understanding what is going on so I can get this chip working.