I'm using TLK2711A chip on a small circuit board to receive the high speed serial signal output by TLK2711-SP on another circuit board.
The PRBS test has passed. The problems is RKLSB and RKMSB of TLK2711A sometimes rise to 1 randomly.
Here is the schematic of the TLK2711A design:
and here is the schematic of the TLK2711-SP design:
We wrongly connected one VDD pin to the GND in the TLK2711-SP design. We've already fixed this error.
Other notes:
1. All the related signals are connected to the GPIO of FPGA.
2. The recovered 100MHz clock can be detected on oscilloscope.
3. we are using dc coupling.
4. We are sure that TKLSB and TKMSB of TLK2711-SP will not rise to 1 erratically, but the RKLSB and RKMSB will rise to 1 erratically.
Can you give us some hints as to where to check? Thank you very much.