Part Number: TCA9509
Other Parts Discussed in Thread: TCA9517,
I have a customer with an I2C application in which either end of the bus wants to be 5V signaling but in between it needs to be 1.8V.
- Can two A ports of a TCA9517 at 1.8V be tied together while each of their B ports at 5V?
- Can the A port of a TCA9517 at 1.8V be tied to the A port of a TCA9509 also at 1.8V or would one need to swap out the TCA9509?
- Would something completely than what is described above me better?