Part Number: DP83826I
Hi
We have a new design where we use DP83826I. We need to use RMII to MAC but the strapping makes us enter MII mode (basic mode and strap10/3/4 all default pulled down to 0)
I thought that all strapping configurations could be changed by SMI register writes after power up. But I am not sure anymore.
First We tried to white SOR2 register but I guess it is Read Only since We can not change the value 0x87.
Is it possible to change from MII to RMII mode after power up with SMI register writes?
I have seen on other phy’s like DP83822 that RCSR register 0x17 bit 5 can be used to charge to RMII mode but on DP83826 this bit is stated as reserved.
Also We have made a hardware patch on our board so that strap4 (COL pin 28) is pulled High. Then We enter RMII mode on power up and everything works just fine.
But to avoid a hardware spin on the board and for understanding of the possibilities of configuration with SMI register writes We would like a description on hon to charge to RMII mode using SMI writes after power up, or some kind of explaination of why it can not be done?
Regards
/Johan