Part Number: DP83867IR
Other Parts Discussed in Thread: DP83869
Hi,
I have questions about DP83867IRPAP Loopback test.
Our customer are testing Analog/MII/Digital loopback with 100Base-TX GMII,
and they are having problem.
They are probing RX_CLK and RX_D[0].Sometimes, the RX_D[0] shows unexpected signal.
This problem occurs in all above loopback test.
Now, we are checking whether the customer's setting procedure is correct.
The DP83867 data sheet and application note do not describe
each loopback setting procedure of 100Base-TX GMII, so we couldn't judge
whether the procedure is correct.
We need to know details of setting procedure of each loopback test.
Could you please provide us each loopback setting procedure of 100Base-TX GMII?
Right now, I'm asking to the customer to try the following procedure for MII loopback,
because they didn't set software reset at first step and
didn't set restart after setting "0xE720" to address 0x00FE.
****************************************************
1.addr:0x001F value:0x8000 //software reset (clears register)
2.addr:0x0000 value:0x6100 //programs DUT to 100BASE-TX mode and enables MII Loopback
3.addr:0x0032 value:0x0000 //Configuration for GMII
4.addr:0x00FE value:0xE720 //Configuration for loopback modes
5.addr:0x001F value:0x4000 //digital restart (doesn’t clear register) end
*****************************************************
By the way, in the application note (SNLA266) of another device (DP83822) page.10 Figure3,
it describes that analog loopback of 100Base-TX and 10Base-Te requires the termination of 100Ω in DP83822.
I can't find any document for DP83867 that is specifically required, but is it also necessary for DP83867IRPAP?
best regards,
g.f.