This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN4550-Q1: There is no INT output signal in TCAN4550-Q1

Part Number: TCAN4550-Q1
Other Parts Discussed in Thread: TCAN4550

Hi Team,

My customer now use TCAN4550-Q1. 

At first, customer found that when receiving large traffic data, there will be frame loss "msg lost in rxf0"

Then customer changed the interrupt thread to receive only one frame at a time to a maximum of 32 frames, and the frame loss problem was solved.

But there is a new problem. When the CAN baud rate is 1M, after running for a period of time, there is no TCAN interrupt signal (INT PIN has no output for SOC) anymore. It seems that TCAN4550 doesn't work at that time.

Could you please kindly help for this?