Part Number: DS90UB953A-Q1
Hello,
I'm developing camera sensor with SER/DES (DS90UB953A / DS90UB954).
New project will be use the 24MP sensor. (5746X4320 Pixel , 10bit raw data, CSI-2 4Lane)
Is it possible to use cropping image sensor as shown below?
full resolution data rate : 5760 x 4320 x 30fps x 10bit = 7.4Gbps ( I think it is over range )
4k resolution data rate : 3714x 2160 x 60fps x 10bit = 4.97Gbps (it possible to use SER/DES) .
Jongpil Chae