Hello everyone,
I have just gotten TDR working on my PHY. I can run the test and, then read the location and amplitude registers. 
However, I am unsure how to scale/interpret these values, as I can find no information in the datasheet on how to do so.
For example, I have a 10 ft CAT6 cable with open termination connected to the PHY. On each of the 4 channels, I see one peak with location = 0b0001 0100 and amplitude = 0b111 1111.
In the data sheet, it says for the amplitude that "The value of these bits is translated into type of cable fault and-or interference." It says something similar for the location.
How do I scale/interpret these values?
Thank you,
Matt