Part Number: TLK2711-SP
I use two TLK2711 for hot swap.
one device is enable and the other device is disable.
The data lines are connected and clock line is also connected.
How much current does each pin draw when the device is shutdown mode?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TLK2711-SP
I use two TLK2711 for hot swap.
one device is enable and the other device is disable.
The data lines are connected and clock line is also connected.
How much current does each pin draw when the device is shutdown mode?
Hi,
Please refer to the shutdown current parameter from datasheet table below.
7.3 Recommended Operating Conditions
over operating free-air temperature range (unless otherwise noted)
|
MIN NOM MAX |
UNIT |
||
|
VDD Supply voltage |
Frequency range 1.6 Gbps to 2 Gbps |
2.375 2.5 2.625 |
V |
|
Frequency range 1.6 Gbps to 2.5 Gbps |
2.5 2.6 2.7 |
||
|
ICC Supply current |
Frequency = 1.6 Gbps, PRBS pattern |
110 |
mA |
|
Frequency = 2.5 Gbps, PRBS pattern |
160 |
||
|
PD Power dissipation |
Frequency = 1.6 Gbps, PRBS pattern |
275 |
mW |
|
Frequency = 2.5 Gbps, PRBS pattern |
400 |
||
|
Frequency = 2.5 Gbps, PRBS pattern |
550 |
||
|
Shutdown current |
Enable = 0, VDDA, VDD pins, VDD = MAX |
3 |
mA |
|
PLL startup lock time |
VDD, VDDC = 2.375 V |
0.1 0.4 |
ms |
|
Data acquisition time |
1024 |
bits |
|
|
Tc Operating case temperature |
–55 125 |
°C |
|
Regards,
Rodrigo Natal
HSSC Applications Engineer