This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN4550: SPI able to read and write to Device ID and SPI Registers only

Part Number: TCAN4550
Other Parts Discussed in Thread: MSP430F5529, ,

Hello,

I am using MSP430F5529 launchpad to communicate with TCAN4550.

I am able to read registers 0x0000, 0x0004, 0x0008, 0x000C only and no other register

After TCAN4x5x_Device_ClearSPIERR(); on reading the next command I am not getting interrupts in 820 register but after that it gives 0x88 error byte.

These are my response on SDI and SDO pins. Also SPI communication works only when clock phase is set 1.

SDI    61 00 0C 01 FF FF FF FF

SDO   88 00 00 00 00 00 00 00

SDI    41 00 0C 01 FF FF FF FF

SDO   00 00 00 00 01 00 00 04

SDI    41 00 00 01 FF FF FF FF

SDO   88 00 00 00 4E 41 43 54

SDI    41 00 04 01 0F 0F 0F 0F

SDO   88 00 00 00 30 35 35 34

SDI    61 08 08 01 AB CD EF 12

SDO   88 00 00 00 00 00 00 00

SDI    41 08 08 01 0F 0F 0F 0F

SDO   88 00 00 00 00 00 00 00

SDI    41 08 20 01 0F 0F 0F 0F

SDO   88 00 00 00 00 00 00 00

* Status register ( 000C ) always gives 0x01000004


my code for setting SPI port.

 UCA0CTL1 |= UCSWRST;                      // **Put state machine in reset**
  UCA0CTL0 |=   UCCKPH + UCMSB + UCMST + UCSYNC;
  UCA0CTL1 |= UCSSEL_2;                     // SMCLK
  UCA0BR0 |= 0x01;                          // /2
  UCA0BR1 = 0;                              //
  UCA0MCTL = 0;                             // No modulation must be cleared for SPI
  UCA0CTL1 &= ~UCSWRST;                     // **Initialize USCI state machine**

and code for clock

    SetVcoreUp (0x01);
     SetVcoreUp (0x02);
     SetVcoreUp (0x03);



    UCSCTL3 = SELREF_2;                       // Set DCO FLL reference = REFO
     UCSCTL4 |= SELA_2;                        // Set ACLK = REFO
     __bis_SR_register(SCG0);                  // Disable the FLL control loop
     UCSCTL0 = 0x0000;                         // Set lowest possible DCOx, MODx
     UCSCTL1 = DCORSEL_5;                      // Select DCO range 50MHz operation
     UCSCTL2 = FLLD_0 + 303;                   // Set DCO Multiplier for 25MHz
     // Set FLL Div = fDCOCLK/2
  __bic_SR_register(SCG0);                  // Enable the FLL control loop
  __delay_cycles(782000);

  // Loop until XT1,XT2 & DCO stabilizes - In this case only DCO has to stabilize
  do
  {
    UCSCTL7 &= ~(XT2OFFG + XT1LFOFFG + DCOFFG);
                                            // Clear XT2,XT1,DCO fault flags
    SFRIFG1 &= ~OFIFG;                      // Clear fault flags
  }while (SFRIFG1&OFIFG);                   // Test oscillator fault flag