Part Number: SN65DP159
Hi TI,
When I use the SN65DP159, I found the regiseter 0B[4:3] can NOT be written.
I have strapped the I2C_EN/PIN to VCC3V3 through a 10K resister,and the let the TX_TERM_CTL No Connext.
And I set the 0x0B=0x89, When I read back the 0x0B, found it is 0x81, the[4:3] can NOT be changed.
WHY? and How can I fix it.
PS: I have another board same as this one. That one can work normally, and this one has NO hdmi data output.
I don't konw the reason.