Part Number: SN65HVD3088E
Hi,
My customer has the following questions. Please answer it.
Termination resistance RL that determines the differential output voltage
(1) In the circuit shown in your data sheet Figure 8, the differential output voltage is 2.3V (typ) when the terminating resistance is RL=54Ω, but how much is output when RL=33.6Ω?
Also, if you select a terminal resistance value other than those listed in the data sheet, may the operation be out of warranty?
(2) It seems that the differential voltage difference will be reduced by making the resistance value of RL smaller than 55Ω. Is there a possibility that wrong operation(H, L error) will occur between SN65HVD3088 transmitter and receiver?
(3) Is half-duplex communication with 110Ω on one side and 55Ω on one side with the circuit shown in the data sheet fig.20, is it operable and within the guaranteed operation?
He is considering Vcc=5V, transmission rate=10Mbps.
Thanks and best regards,
M.HATTORI.