Part Number: TUSB321AI
Other Parts Discussed in Thread: TUSB321, TUSB211, TPS25910, TUSB542
Hi Team,
My customer would like to use TUSB321AI in his system as UFP port. He tested its function on TUSB524 EVM but the result is not as expected.
The EVM's type-C port was connected to a NB( HP zbook15g3) and NB's type-C port can support 5V/3A. Supposedly, both CC1 and CC2 should output low level but customer probed that the CC1 is at high level, CC2 is at low level.
https://pcase.pl/site_media/uploads/hp/ZBook15G3/HP-ZBook-15-G3.pdf
Customer removed U5(TPS25910), U6(TUSB211) out of the EVM, pull TUSB321 pin 4 to ground as UFP mode. Connecting VBUS_B and VBUS_C. Then probed OUT1/OUT2 signal level.
Ask customer to probe CC1/CC2/VBUS/OUT1 and CC1/CC2/OUT1/OUT2 waveform as following.
Could team help to comment why the result is not as expected? Any experiment we can do here?
Thanks a lot.
Vincent Chen