Hii
I was using the TCAN1042 IC in one of my application. Recently we found that in 3 PCBA's CANH and CANL are showing low resistance w.r.t ground(in ohm). we have TVS diodes(SZNUP2105LT1G) on CANH and CANL lines(placed near to connector). Also we have common mode choke(ACT45B-220-2P-TL003). when i measure the TVS it is healthy. when I replaced the CAN IC system working fine. I need to understand at what situation this problem will occurs.
1) Power supply to IC cannot go more than 5.3V. if it goes above uC will shunt down the system.
2) I have checked the placement of TVS. it is near to connector and differential lines are taken care such that if any surge comes TVS will react.
Can I know at what are all condition this problem can occur
Also can i get the document which i mentioned in the below comments
Hi Mitchell,
Unfortunately I don't, and because of some weather-related issues with our lab at the moment I'm not able to capture these (the other waveforms I had on hand already). I can tell you that if CANH is shorted to CANL, the differential voltage between them will be 0 V and the receiver will only report a recessive state on the bus.
If you think through the different possible shorting scenarios, you can predict the device behavior based on its performance as documented in the datasheet. Understanding the behavior of the device in this way is better in my opinion that trusting in the results of a single measurement (with its assumptions related to battery voltages, other nodes on the bus, shorting impedances, etc.). I've put together a document that describes how a transceiver would behave under different system-level fault conditions. I will send it to you via e-mail, and hopefully that can be used to give some better confidence in the part.
Regards,
Max
Regards
Bharath Gilla