Part Number: TCA6408A
Hi Sir,
Would you pls help below questions for schematic design? thanks.
1. P0 and P2–P4 are configured as inputs.
--> These 4pins only can be input?
2. P1 and P5–P7 are configured as outputs.
-->These 4pins only can be output?
3. Resistors are required for inputs (on P-port) that may float. If a driver to an input will never let the input float, a resistor
is not needed. Outputs (in the P-port) do not need pull-up resistors.
--> will it keep High or Low after power on? If input need to have pull-up resistors?
4. If INT/RST need to add pull-up resistors?
And pls kindly help review below schematic, thanks.
Thanks, Ian.