Hello to all,
in our application out box must be silent during power up and during the power-up phase existing communication shall be not disturbed or corrupted.
In case of this the data sheet describes not clearly the power-up behaviour of this CAN-Transceiver (or I have not found the chapter).
The question is;
a) during power up of the 5V supply source how is the reaction of the external transceiver I/O's CANH and CANL in the supply voltage range from 0V to < Vcc_min ?
Can we expect that these IO's will not impact the CAN bus?
b) during power up of the VIO supply source, how is the behaviour of the transceiver IO's CANH and CANL in the supply voltage range from 0V to <VIO_min ?
Can we expect that these IO's will not impact the CAN bus?
My concern is, that the data sheet defines only when Vcc = VIO = 0V the then only the max. leakage current is flowing. But for the range between 0V and the min. supply voltage exists no statement.
Would be happy to get soon a reliable answer about my problem.
Thank you in advance
Norbert