Part Number: SN65HVD10-EP
Other Parts Discussed in Thread: SN65HVD10, THVD2450, THVD1450
I am analyzing a SN65HVD10MDREP in a circuit that has external protection on the outputs of the device. I need the characteristics of the internal 16V clamps to determine if my circuit will pass or not. Does anyone have the room temperature tolerance, the temperature coefficient and effective series impedance available for the 16V internal clamps? Or is a plot of voltage vs current on the 16V clamps available? I need to analyze it in a circuit that doesn't have a series 100 ohm with the applied voltage transient