Part Number: AM26C31
Other Parts Discussed in Thread: THVD1410, THVD1450
I am working on an application where we need to have two controllers which can control a single RS422 device, at the moment we are considering using an AM26C31 to drive the RS422 lines. One controller is there for redundancy and will never be switched on whilst the other is turned on. If one controller is faulty, it will be powered down then the second will be powered up.
I have read SLLA070D but it is still unclear if it is possible to have two masters electrically connected on the bus if only one will ever be active, and if it is possible where the termination resistors should go?